:LLINe:SOURce
Command Syntax
:LLINeN:SOURce <source_waveform>
Where N identifies one of 64 {1:64} possible limit lines. For example, :LLINe23.
Where <source_waveform> can be one of the following:
CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply useCHANnel<ch1-8>.CGMemory{1:8}FUNCtion{1:64}
Query Syntax
:LLINeN:SOURce?
Description
Selects the source waveform on with to apply a Limit Line Test.
Example
:LLINe8:SOURce CHANnel1_2