:LLINe Subsystem

Use the :LLINe subsystem commands to load, display, and horizontally position a Limit-Line Test file. There are no commands for creating limit lines. Limit lines provide pass/fail testing on single-valued waveforms. A data point "passes" if it is inside the displayed limit lines and "fails" is it is beyond the limit lines. Once loaded, you can shift the limit line relative to the waveform along the time scale. Limit Lines Tests are created using an ASCII editor.

Use the :LTESt subsystem to stop limit testing on the first passed or failed data point and to report the results.

Commands