:LTESt:MEASure:SIMage:FNAMe:USTandard
Command Syntax
:LTESt:MEASure:SIMage:FNAMe:USTandard
Description
Resets the file name for the screen image file from using a custom name to using the standard name in the following form:
Screen_<date><autonumber>.<extension>
For example, Screen_2017-04-08_1.jpg. Refer to :LTESt:MEASure:SIMage:FNAMe to learn about standard and custom names.