:LTESt:MEASure:SIMage:MONochrome

Command Syntax

:LTESt:MEASure:SIMage:MONochrome {ON | OFF | 1 | 0}

Query Syntax

:LTESt:MEASure:SIMage:MONochrome?

Query Response

{1 | 0}

Description

Turns monochrome screen capture on and off when reporting a screen capture for a measurement limit test. When on, a black and white image will be captured and saved into a file by the :LTESt:MEASure:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color. Use the :LTESt:MEASure:SIMage:STATe command to enable screen captures to be saved when the limit test completes.