:LTESt:MEASure:SIMage:STATe

Command Syntax

:LTESt:MEASure:SIMage:STATe {ON | OFF | 1 | 0}

Query Syntax

:LTESt:MEASure:SIMage:STATe?

Query Response

{1 | 0}

Description

Selects to save a screen image to a file after the specified number of measurement failures stops the limit test.

Information on identifying the measurement is found in the introduction to the limit test programming subsystem. Use the commands shown in the following table to configure the output file.

Commands to Configure the Output
Task Command
Enter the filename and path :LTESt:MEASure:SIMage:FNAMe
Enter the graphics file type :LTESt:MEASure:SIMage:FTYPe?
Select portion of Infiniium display to capture :LTESt:MEASure:SIMage:WINDow
Include metadata in jpg and tiff files. :LTESt:MEASure:SIMage:IMETadata
Invert background color :LTESt:MEASure:SIMage:INVert
Black and white output :LTESt:MEASure:SIMage:MONochrome
Capture a single waveform among several displayed waveforms :LTESt:MEASure:SIMage:SINClude