:LTESt:MEASure:SIMage:WINDow

Command Syntax

:LTESt:ACQuire:SIMage:WINDow  {DISPlay | TIME{1} | SHERtz{1:4} | DBHertz{1:4} | DHERtz{1:4}}

Query Syntax

:LTESt:ACQuire:SIMage:WINDow?

Query Response

{1 | 0}

Description

When reporting a screen image as a result of an measurement limit test, use this command to selects which portion of the screen to include in the image. To actually specify that a screen image is saved, use the :LTESt:MEASure:SIMage:STATe command. The following selections are available:

DISPlay
Includes the entire Infiniium 2026 screen in the captured screen image.
TIMe1
Includes only the Waveform content window in the captured screen image.
SHERtz{1:4}
Includes only the Delay 1, Delay 2, Delay 3, or Delay 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Delay windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Delay window can be selected as a display output format for FFT functions (:FUNCtion:FOPerator FFT).
DBHertz{1:4}
Includes only the Decibels (Hz) 1, Decibels (Hz) 2, Decibels (Hz) 3, or Decibels (Hz) 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Decibels (Hz) windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Decibels (Hz) window can be selected as a display output format for FFT functions (:FUNCtion:FOPerator FFT).
DHERtz{1:4}
Includes only the Degrees (Hz) 1, Degrees (Hz) 2, Degrees (Hz) 3, or Degrees (Hz) 4 content window in the captured screen image. This selection is only available if one of these windows is actually displayed. Degrees (Hz) windows 2, 3, and 4 can only be displayed programmatically and not using front-panel controls. The group Degrees (Hz) window can be selected as a display output format for FFT functions (:FUNCtion:FOPerator FFT).