:MARKer:X:SOURce:DUT
Command Syntax
:MARKer:XN:SOURce:DUT {DUT{1:16}}
Where N identifies one of four {1:4} markers. For example, :MARKer2.
Description
Use this command along with the :MARKer:X:SOURce:SPARameter command to select a tracking marker's S-parameter. This command applies only to tracking markers and does not affect manual line markers.
Query Syntax
:MARKer:XN:SOURce:DUT?