:MARKer:X:SOURce:SPARameter

Command Syntax

:MARKer:XN:SOURce:SPARameter <parameter>

Where N identifies one of four {1:4} markers. For example, :MARKer2.

The <parameter> argument is an S-parameter name with an underscore (_) character between the numbers. For example, the argument for an S21 parameter is S2_1.

Description

Use this command along with the :MARKer:X:SOURce:DUT command to select a tracking marker's S-parameter memory source waveform. This command selects the S-parameter. This command applies only to tracking markers and does not affect manual line markers.

Query Syntax

:MARKer:XN:SOURce:SPARameter?

Parent Command