:MARKer:Y:SOURce
Command Syntax
:MARKer:YN:SOURce {CHANnel{N} | DIFF{1:4} | FUNCtion{1:64} | WMEMory{1:8} | TRACe{1:128}
| ECHannel{N} | EDIFf{1:4} | EFUNction{1:64} | EWMemory{1:8} | CGMemory{1:8}}
In the command syntax, Y1A, Y2A, Y3A, and Y4A select the marker.
Real-time eye sources are available for manual line markers only.
Query Syntax
:MARKer:YN:SOURce?
Description
Selects the source waveform for one of four tracking markers. Using the :MARKer:X:SOURce command achieves the same result. Sources can be channels, differential waveforms, functions, traces, and waveform memories.
This command has no effect on manual line markers.
Example Command Sequence
This example illustrates how to use all of the marker related commands and, as a result, is not presented as a best measurement practice. The example uses a tracking marker, manual line X marker, and manual line Y marker. Because a tracking marker is used, the waveforms must be single-valued. You could also turn on two tracking markers and read the delta values between them.
// Configure Manual Line Marker X1
:MARKer:X1:STATe MANual // Turn on marker
:MARKer:X1:SOURce CHAN1_1 // Assign marker to connection 1 channel 1 waveform
:MARKer:X1:POSition 80E-12 // Position marker to 80 ps
// Configure Manual Line Marker Y1
:MARKer:Y1A:STATe MANual // Turn on Y manual line marker 1.
:MARKer:Y1A:SOURce CHAN1_1 // Assign marker to connection 1 channel 1 waveform
:MARKer:Y1A:POSition 120E-3 // Position marker to 120 mv
:MARKer:REFerence X1 // Set markers X1 and Y1 as the reference
// Configure Tracking Marker Pair 2
:MARKer:Y2A:STATe TRACking // Turn on marker
:MARKer:X2:SOURce FUNCtion3 // Assign marker to FUNCtion3 waveform
:MARKer:X2:POSition 200E-12 // Position marker on screen
… // Prompt tester to position marker on the waveform
// Return Marker Table Measurements for Tracking Marker 2
:MEASure:MARKer:DX2? // Return ΔPosition
:MEASure:MARKer:IDX2? // Return inverse of ΔPosition
:MEASure:MARKer:DY2A? // Return ΔMagnitude
:MEASure:MARKer:Y2A? // Return Y2 Magnitude