:MARKer:Y:SOURce:DUT
Command Syntax
:MARKer:YN:SOURce:DUT {DUT{1:16}}
Where N identifies one of four markers {1:4}{A|B|C}. For example, .:MARKer2B
Description
This command controls the same setting as :MARKer:X:SOURce:DUT command, which should be used instead to encourage consistency. Because manual line markers cannot be placed on S-parameter waveforms, this command applies only to tracking markers.