:MEASure:EYE:PAM:VECLosure:DEFine:EOPening
Command Syntax
:MEASure:EYE:PAM:VECLosure:DEFine:EOPening {ZHITs | PROBability}
Query Syntax
:MEASure:EYE:PAM:VECLosure:DEFine:EOPening?
Query Response
{ZHIT | PROB}
Description
Selects the Eye Opening Definition for the :MEASure:EYE:PAM:VECLosure measurement to be either the Zero Hits (ZHIT) or At Probability (PROBability). The default Eye Opening Probability is 10–6. When PROBability is specified, use the following child commands to define the probability:
:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBabilityenters the probability.