:MEASure:EYE:PAM:VECLosure:LOCation?
Query Syntax
:MEASure:EYE:PAM:VECLosure:LOCation?
Description
Returns an location index of the :MEASure:EYE:PAM:VECLosure measurement for PAM signals in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.