:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability
Command Syntax
:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability <double>
Where <double> is a probability.
Query Syntax
:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability?
Description
Enters a value of Eye Opening Probability to be used when the VEC measurement's Eye Opening Definition is set to At Probability (:MEASure:EYE:PAM:VECLosure:DEFine:EOPening).