:MEASure:EYE:PAM:VECLosure:EYE
Command Syntax
:MEASure:EYE:PAM:VECLosure:EYE {EYE0}
Query Syntax
:MEASure:EYE:PAM:VECLosure:EYE?
Query Response
{EYE0}
Description
This command allows you to select an eye on PAM signals. For NRZ signals, the 0 eye is automatically selected and cannot be changed. The command selects the PAM eye on which to perform the :MEASure:EYE:PAM:VECLosure. The query form of the command returns the currently selected eye.