:MEASure:FFT:THDistortion:FFFRequency

Command Syntax

:MEASure:FFT:THDistortion:FFFRequency <fundamental_freq>

<fundamental_freq> is a double.

Query Syntax

:MEASure:FFT:THDistortion:FFFRequency?

Description

When the mode of specifying the fundamental frequency for the Total Harmonic Distortion measurement (:MEASure:FFT:THDistortion:FFFMode) is MANual, this command specifies the fundamental frequency.