:MEASure:FFT:THDistortion:FPLevel

Command Syntax

:MEASure:FFT:THDistortion:FPLevel <dBm>

<dBm> is a double.

Query Syntax

:MEASure:FFT:THDistortion:FPLevel?

Description

Defines the threshold an FFT peak must cross to be considered a peak in the Total Harmonic Distortion measurement (:MEASure:FFT:THDistortion). The default Peak Level is -40 dBm.