:MEASure:FFT:THDistortion:FPNumber

Command Syntax

:MEASure:FFT:THDistortion:FPNumber <peak_number>

<peak_number> is an integer.

Query Syntax

:MEASure:FFT:THDistortion:FPNumber?

Description

When the mode of specifying the fundamental frequency for the Total Harmonic Distortion measurement (:MEASure:FFT:THDistortion:FFFMode) is FPEak, this command specifies the peak number to use when determining the fundamental frequency.

The specified peak level (:MEASure:FFT:THDistortion:FPLevel) is used in determining the frequency peaks and peak numbering.