:MEASure:HORizontal:TEDGe
Command Syntax
:MEASure:HORizontal:TEDGe
Query Syntax
:MEASure:HORizontal:TEDGe?
Description
Moves the Time-at-Edge measurement to the top of the Results table. Displays the measurement if it is not already shown on the table. The query form of the command returns the measured value. Time-at-Edge is the measure of the time at which the specified waveform edge occurs on the displayed waveform. To specify the edge, use the :MEASure:HORizontal:TEDGe:NUMBer child command. Specify a rising or falling edge with the :MEASure:HORizontal:TEDGe:EDIRection command. Specify the edge threshold with the :MEASure:HORizontal:TEDGe:THReshold child command. Sources can be any displayed waveform, waveform memory, or function. For example, CHAN1_1, WMEMory1, or FUNCtion1. Use :MEASure:TBASe:GENeral:METHod to change the definition of the waveform's top/base. Use :<waveform>:THReshold:GENeral:METHod to change the definition of the waveform's threshold.
PAM Compatibility. Because this measurement is based on waveform top and base levels and the passing of the waveform's edge through lower, middle, and upper thresholds, the measurement is not designed for PAM signals. However, the measurement may be able to be made on PAM signals if the waveform top and base definitions are manually set. This can be attempted using the following commands: :MEASure:TBASe:GENeral:METHod, :CHANnel:THReshold:GENeral:TOP, and :CHANnel:THReshold:GENeral:BASE commands.
Example Command Sequence
:MEASure:HORizontal:TEDGe:SOURce CHAN2_2 :MEASure:HORizontal:TEDGe:EDIRection RISing :MEASure:HORizontal:TEDGe:NUMBer 2 :MEASure:HORizontal:TEDGe:THReshold MIDDle :MEASure:HORizontal:TEDGe :MEASure:HORizontal:TEDGe?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Infiniium.query(':MEASure:HORizontal:TEDGe:STATus?')):
measurement = Infiniium.query(':MEASure:HORizontal:TEDGe?')
If averaging is turned on (:ACQuire:SMODe AVERage), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:COUNt?) versus the number of measurement sweeps that have occurred (:ACQuire:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Infiniium.query(':MEASure:HORizontal:TEDGe:COUNt?') >= Infiniium.query(':ACQuire:COUNt?')):
measurement = Infiniium.query(':MEASure:HORizontal:TEDGe?')
You can also use an acquisition limit test to test that a number of waveforms or samples have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Querying Measurement Results and Statistics
You can query measurement results using the :MEASure:HORizontal:TEDGe? query after making the proper instance settings.
If a measurement is installed into Results table (using the :MEASure:HORizontal:TEDGe command) and you have made the proper instance settings, you can query statistics using common child queries.
Also, you can query measurement results and statistics directly from the Results table (without having to make the proper instance settings beforehand). See Querying Measurement Results and Statistics.