:MEASure:HORizontal:TEDGe:THReshold
Command Syntax
:MEASure:HORizontal:TEDGe:THReshold {UPPer | MIDDle | LOWer}
Query Syntax
:MEASure:HORizontal:TEDGe:THReshold?
Description
For the Time-at-Edge measurement, specifies the edge threshold used to identify the waveform's edge: upper, middle, or lower. To specify the edge number, use the :MEASure:HORizontal:TEDGe:NUMBer command. To specify the edge direction, use the :MEASure:HORizontal:TEDGe:EDIRection command.
Example Command Sequence
:MEASure:HORizontal:TEDGe:SOURce CHAN2_2 :MEASure:HORizontal:TEDGe:EDIRection RISing :MEASure:HORizontal:TEDGe:NUMBer 2 :MEASure:HORizontal:TEDGe:THReshold MIDDle :MEASure:HORizontal:TEDGe :MEASure:HORizontal:TEDGe?