:MEASure:HORizontal:TEDGe:NUMBer
Command Syntax
:MEASure:HORizontal:TEDGe:NUMBer <edge_number>
<edge_number> is an int.
Query Syntax
:MEASure:HORizontal:TEDGe:NUMBer?
Description
For the Time-at-Edge measurement, specifies the edge number used to identify the waveform's edge. To specify the edge threshold, use the :MEASure:HORizontal:TEDGe:THReshold command. To specify the edge direction, use the :MEASure:HORizontal:TEDGe:EDIRection command.
Example Command Sequence
:MEASure:HORizontal:TEDGe:SOURce CHAN2_2 :MEASure:HORizontal:TEDGe:EDIRection RISing :MEASure:HORizontal:TEDGe:NUMBer 2 :MEASure:HORizontal:TEDGe:THReshold MIDDle :MEASure:HORizontal:TEDGe :MEASure:HORizontal:TEDGe?