:MEASure:HORizontal:TEDGe:EDIRection

Command Syntax

:MEASure:HORizontal:TEDGe:EDIRection  {RISing | FALLing}

Query Syntax

:MEASure:HORizontal:TEDGe:EDIRection?

Description

For the Time-at-Edge measurement, specifies the edge direction used to identify the waveform's edge: rising or falling. To specify the edge number, use the :MEASure:HORizontal:TEDGe:NUMBer command. To specify the edge threshold, use the :MEASure:HORizontal:TEDGe:THReshold command.

Example Command Sequence

:MEASure:HORizontal:TEDGe:SOURce CHAN2_2
:MEASure:HORizontal:TEDGe:EDIRection RISing
:MEASure:HORizontal:TEDGe:NUMBer 2
:MEASure:HORizontal:TEDGe:THReshold MIDDle
:MEASure:HORizontal:TEDGe
:MEASure:HORizontal:TEDGe?