:MEASure:JITTer:JITTer:GRAPh:JSPectrum

Command Syntax

:MEASure:JITTerN:JITTer:GRAPh:JSPectrum {ON | OFF | 1 | 0}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:JITTer:GRAPh:JSPectrum?

Query Response

{1 | 0}

Description

Enables or disables the Aliased Jitter Spectrum jitter graph.