:MEASure:JITTer:JITTer:MGRaph
Command Syntax
:MEASure:JITTerN:JITTer:MGRaph {RJPJhist | TJHist | DDJHist | JBAThtub
| SVTFit | DDJSymbol | IFILter | JSPectrum | CTJHist | CDDJhist}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:JITTer:MGRaph?
Description
This command selects the Jitter graph that should be maximized in the graph display area when using the :MEASure:JITTer:JITTer:DMAXimized command:
RJPJhist— RJ/PJ HistogramTJHist— TJ HistogramDDJHist— DDJ HistogramJBAThtub— Jitter BathtubSVTFit— Jitter Spectrum versus Tail FitDDJSymbol— DDJ vs SymbolIFILter— ISI FilterJSPectrum— Aliased Jitter SpectrumCTJHist— Composite TJ HistogramCDDJhist— Composite DDJ Histogram