:MEASure:JITTer:JITTer:GSIZe
Command Syntax
:MEASure:JITTerN:JITTer:GSIZe {SMALl | MEDium | LARGe | OGRaph | OBTWo
| TBONe | TWBTwo | TBTHree | TBTWo | THBThree}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:JITTer:GSIZe?
Description
This command selects the graph size option in the Jitter results content window:
SMALl— Auto fit smallMEDium— Auto fit mediumLARGe— Auto fit largeOGRaph— One graphOBTWo— 1x2TBONe— 2x1TWBTwo— 2x2TBTHree— 2x3TBTWo— 3x2THBThree— 3x3