:MEASure:JITTer:JITTer:GRAPh:RPSPectrum
Command Syntax
:MEASure:JITTerN:JITTer:GRAPh:RPSPectrum {ON | OFF | 1 | 0}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:JITTer:GRAPh:RPSPectrum?
Query Response
{1 | 0}
Description
Enables or disables the RJ,PJ Spectrum jitter graph.