:MEASure:MTESt:THRegion:STATus:DETails?
Query Syntax
:MEASure:MTESt{N}:THRegion:STATus:DETails?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Description
Returns a string that may provide additional details for a failed :MEASure:MTESt:THRegion{N}? measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:MTESt:THRegion{N}:STATus:REASon? sibling query. Use the :MEASure:MTESt:THRegion{N}:STATus? parent query to determine if the measurement has failed.