:MEASure:MTESt:THRegion{N}:STATus:REASon?
Query Syntax
:MEASure:MTESt{N}:THRegion{1:16}:STATus:REASon?
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2 selects mask 2.
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for a failed :MEASure:MTESt:THRegion{N}? measurement. If the measurement was successful, a null string is returned.
Additional information about the failure may be available using the :MEASure:MTESt:THRegion:STATus:DETails? sibling query. Use the :MEASure:MTESt:THRegion{N}:STATus? parent query to determine if the measurement has failed.