:MEASure:PAM:EYE:ELMethod
Command Syntax
:MEASure:PAM:EYE:ELMethod {MEWidth | MEHeight}
Description
Selects the basis for determining the location of an eye's center on the waveform. This setting affects all PAM eye measurements. It does not affect PAM waveform measurements.
| Arguments | Description |
|---|---|
| MEWidth | The eye's center is located at the eye's maximum width midway between the eye's inside left and right edges. This is the default setting. |
| MEHeight | The eye's center is located at the eye's maximum height midway between the eye's inside top and bottom edges. |