:MEASure:PAM:EYE:PPERcent

Command Syntax

:MEASure:PAM:EYE:PPERcent <% value>

<% value> is a double.

Query Syntax

:MEASure:PAM:EYE:PPERcent?

Description

Defines the timespan over which an eye's amplitude level is measured. The timespan is specified as a percentage of the symbol period. The default setting is 10%. This setting affects all PAM eye measurements except Eye Widths (:MEASure:EYE:PAM:EWIDth). It does not affect PAM waveform measurements.