:MEASure:PAM:EYE:TIME:UNITs

Command Syntax

:MEASure:PAM:EYE:TIME:UNITs {SECond | UINTerval}

Query Syntax

:MEASure:PAM:EYE:TIME:UNITs?

Description

Sets the time units for PAM width and skew measurements. The units can be seconds (SECond) or unit interval (UINTerval). The following measurements are affected by this setting: