:MEASure:PAM:AMPLitude:UNITs

Command Syntax

:MEASure:PAM:AMPLitude:UNITs {AMPLitude | PERCent}

Description

Sets the amplitude units for PAM level and level RMS (thickness) measurements. The selections are amplitude (volts or Watts) or percent. The following measurements are affected by this setting:

To select the units for Jitter measurements (seconds or unit interval), use the :MEASure:JITTer:JITTer:UNITs command.