:MEASure:PJITter:DDIRac:SIZE?

Query Syntax

:MEASure:PJITterN:DDIRac:SIZE?

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Description

This query returns the number of edges defined in the PAM Jitter definition.

For the PCIe Dual-Dirac 52-symbol pattern, 48 edges are defined.