:NETWorks:TRACe:CWINdow

Command Syntax

:NETWorks:TRACeN:CWINdow {TPERcent{1:4} | TVOLts{1:4} | TOHMs{1:4} | DBHertz{1:4}
   | DHERtz{1:4} | SHERtz{1:4} | IRESponse{1:4} | SRESponse{1:4}}

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACe{1:128}:CWINdow?

Description

When multiple S-parameter file or transfer function file parameter traces are displayed in a content window, this command moves a trace to a content window of the same type. If the content window does not already exist, it will be created. For example, consider that an S21 trace from one DUT and an S21 from another DUT are both displayed in a Degrees (Hz) content window. The :CWINdow command can be used to move one trace to an new second Degrees (Hz) content window. Up to four content windows of the same type can be created.

Example Command Sequence

// Create Trace 1 (S21) from DUT 1.
:NETWorks:TRACe1:PARameter S2_1
:NETWorks:TRACe1:OPERator PHASe  //  Display in Degrees (Hz) content window.
:NETWorks:TRACe1:COLor TCOLor2
:NETWorks:TRACe1:DISPlay ON

// Create Trace 2 (S21) from DUT 2.
:NETWorks:TRACe2:PARameter S2_1
:NETWorks:TRACe2:OPERator PHASe  //  Display in the same Degrees (Hz) content window as Trace 1.
:NETWorks:TRACe2:COLor TCOLor3
:NETWorks:TRACe2:DISPlay ON

  //  Move Trace 2 to a new Degrees (Hz) content window (number 2).
:NETWorks:TRACe2:CWINdow DHERtz2