:NETWorks:TRACe:NETWork

Command Syntax

:NETWorks:TRACeN:NETWork SPMemory{1:4}

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACe{1:128}:NETWork?

Description

This command specifies an S-parameter or transfer function memory from which to select a response to assign to a trace. One of four S-parameter/transfer function file memories can be selected as the source for a response. To select the actual S-parameter/transfer function response to assign to the trace, use the :NETWorks:TRACe:PARameter command.