:NETWorks:TRACe:OPERator

Command Syntax

:NETWorks:TRACeN:OPERator {NONE | OHMS | VOLTs | PERCent | MAGNitude | PHASe | GDELay
   | IRESponse | SRESponse}

Where N identifies a specific trace and must be selected from 1 to 128 {1:128}.

Query Syntax

:NETWorks:TRACe{1:128}:OPERator?

Description

Specifies the type of graph in which to display an S-parameter or transfer function trace. The following table shows the content window graph selected by each command argument. An S-parameter or transfer function trace can also be displayed in one of three or five content windows. To display the same parameter in all multiple graphs, define multiple separate traces. Use the :NETWorks:TRACe:PARameter command to assign the actual parameter to the trace.

Arguments with Displayed Content Windows
Command
Argument
Content Windows
S-Parameters Transfer Function
MAGNitude Decibels (Hz) Decibels (Hz)
PHASe Degrees (Hz) Degrees (Hz)
GDELay Seconds (Hz) Seconds (Hz)
IRESponse   Impulse Response
SRESponse   Step Response