:TIMebase:FINE

Command Syntax

:TIMebase:FINE {{OFF | 0} | {ON | 1}}

Query Syntax

:TIMebase:FINE?

Query Response

{0 | 1}

Description

Enables or disables fine adjustment of the horizontal scale.

When OFF (coarse adjustment), the horizontal scale is adjusted in a 1-2-5 sequence.

When ON (fine adjustment), the horizontal scale is adjusted in smaller, evenly spaced increments.