:TIMebase:XRANge

Command Syntax

:TIMebase:XRANge  <range>

<range> is a double.

Query Syntax

:TIMebase:XRANge?

Description

Sets or queries the full-scale horizontal time in seconds (span between the graticule left and right edges). Use :TIMebase:XLEFt? to query the time value at the graticule's left edge, :TIMebase:XRIGht? to query the time value at the graticule's right edge, and :TIMebase:SCALe to set the time-per-division setting.