:TIMebase:SCALe

Command Syntax

:TIMebase:SCALe  <seconds>

<seconds> is a double.

Query Syntax

:TIMebase:SCALe?

Description

Sets the horizontal timebase scale in seconds-per-division, when the timebase units are set to seconds ( ). To change the timebase scale to symbols instead of seconds, use  . Use the :TIMebase:XLEFt? to query the time value at the graticule's left edge and :TIMebase:XRANge to set the time span across the graticule from the left edge to the right edge.

Common Numerical Child Commands

This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.

Example Command Sequence

:TIMebase:SCALe 5.02E-12
:TIMebase:POSition 2.41E-08