:TRIGger:PATTern:REND
Command Syntax
:TRIGger:PATTern:REND <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:PATTern:REND?
Description
In the Pattern trigger mode (see :TRIGger:MODE), when triggering when the pattern is inside or outside a range (see :TRIGger:PATTern:MODE), this command specifies the time range ending time.