:TRIGger:PATTern:TIME
Command Syntax
:TRIGger:PATTern:TIME <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:PATTern:TIME?
Description
In the Pattern trigger mode (see :TRIGger:MODE), when triggering when the pattern is present for less than or greater than a specified time (see :TRIGger:PATTern:MODE), this command specifies the amount of time.