:TRIGger:PATTern:RSTart

Command Syntax

:TRIGger:PATTern:RSTart <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:PATTern:RSTart?

Description

In the Pattern trigger mode (see :TRIGger:MODE), when triggering on a transition that is inside or outside a time range (see :TRIGger:TRANsition:MODE), this command specifies the range start time.