:TRIGger:SEQuence:DELay:ARM:SLOPe
Command Syntax
:TRIGger:SEQuence{A|B}:DELay:ARM:SLOPe {POSitive | NEGative}
Query Syntax
:TRIGger:SEQuence{A|B}:DELay:ARM:SLOPe?
Description
In the Edge Then Edge trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the edge of the Arm Source (see :TRIGger:SEQuence:DELay:ARM:SOURce) that will arm the trigger.