:TRIGger:SEQuence:DELay:EDELay:COUNt
Command Syntax
:TRIGger:SEQuence{A|B}:DELay:EDELay:COUNt <occurrences>
<occurrences> is an int.
Query Syntax
:TRIGger:SEQuence{A|B}:DELay:EDELay:COUNt?
Description
In the Edge Then Edge trigger mode (see :TRIGger:SEQuence:MODE), when Delaying By Event (see :TRIGger:SEQuence:DELay:MODE), this command specifies the number of occurrences of the specified edge event that will qualify the delay.