:TRIGger:SEQuence:DELay:TDELay:TIME

Command Syntax

:TRIGger:SEQuence{A|B}:DELay:TDELay:TIME <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:DELay:TDELay:TIME?

Description

In the Edge Then Edge trigger mode (see :TRIGger:SEQuence:MODE), when Delaying By Time (see :TRIGger:SEQuence:DELay:MODE), this command specifies the amount of time that will qualify the delay.