:TRIGger:SEQuence:DELay:TRIGger:COUNt

Command Syntax

:TRIGger:SEQuence{A|B}:DELay:TRIGger:COUNt  <occurrences>

<occurrences> is an int.

Query Syntax

:TRIGger:SEQuence{A|B}:DELay:TRIGger:COUNt?

Description

In the Edge Then Edge trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the Nth occurrence of the trigger source edge that will trigger.