:TRIGger:SEQuence:PATTern:MODE
Command Syntax
:TRIGger:SEQuence{A|B}:PATTern:MODE {ENTered | EXITed | LTHan | GTEXit | GTTout | RINSide | ROUTside
| TPANd | TPNand}
Query Syntax
:TRIGger:SEQuence:PATTern:MODE?
Description
In the Pattern trigger mode (see :TRIGger:SEQuence:MODE), this command selects the time the pattern must be present for in order to cause a trigger.
When the pattern consists of logic levels only, you have these options:
ENTered— Triggers on the edge of the signal that makes the pattern true.EXITed— Triggers on the edge of the signal that makes the pattern false.LTHan— Triggers when the pattern is present for less than the specified:TRIGger:SEQuence:PATTern:TIME.GTEXit— When the pattern is present for greater than the specified:TRIGger:SEQuence:PATTern:TIME, triggers when the pattern ends (on the signal edge that makes the pattern invalid).GTTout— When the pattern is present for greater than the specified:TRIGger:SEQuence:PATTern:TIME, triggers when the time is exceeded.RINSide— Trigger when the pattern is present for a time within the range specified by the:TRIGger:SEQuence:PATTern:RSTartand:TRIGger:SEQuence:PATTern:RENDvalues. The trigger occurs on the signal edge that makes the pattern invalid (like "on Exit").ROUTside— Trigger when the pattern is present for a time outside the range specified by the:TRIGger:SEQuence:PATTern:RSTartand:TRIGger:SEQuence:PATTern:RENDvalues.
When the pattern includes an edge identifier, you have these options:
TPANd— The trigger point is the edge AND the pattern on the remaining channels.TPNand— The trigger point is the edge AND NOT the pattern on the remaining channels.
Edges are identified when a signal passes through the trigger threshold voltage. The direction of the edge is determined based on hysteresis around the trigger threshold.
The combination of an edge and a pattern is known as a State trigger.