:TRIGger:SEQuence:PATTern:REND

Command Syntax

:TRIGger:SEQuence{A|B}:PATTern:REND <seconds>

<seconds> is a double.

Query Syntax

:TRIGger:SEQuence{A|B}:PATTern:REND?

Description

In the Pattern trigger mode (see :TRIGger:SEQuence:MODE), when triggering when the pattern is inside or outside a range (see :TRIGger:SEQuence:PATTern:MODE), this command specifies the time range ending time.