:TRIGger:SEQuence:PATTern:RSTart
Command Syntax
:TRIGger:SEQuence{A|B}:PATTern:RSTart <seconds>
<seconds> is a double.
Query Syntax
:TRIGger:SEQuence{A|B}:PATTern:RSTart?
Description
In the Pattern trigger mode (see :TRIGger:SEQuence:MODE), when triggering on a transition that is inside or outside a time range (see :TRIGger:SEQuence:TRANsition:MODE), this command specifies the range start time.