:TRIGger:SEQuence:CHANnel:PATTern:STATe
Command Syntax
:TRIGger:SEQuence{A|B}:CHANnelN:PATTern:STATe {HIGH | LOW | DCARe | RSLope | FSLope | ESLope}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:TRIGger:SEQuence:CHANnelN:PATTern:STATe?
Description
For the specified input channel, this channel selects the logic level or edge that should be included in the pattern:
-
HIGH— Logic level 1. A value is considered a 1 (high) when the waveform's voltage level is greater than its trigger threshold level. -
LOW— Logic level 0. A value is considered a 0 (low) when the waveform's voltage level is less than its trigger threshold level -
DCARe— Don't care (logic level 1 or 0). If a channel is set to X (don't care), it is not used as part of the pattern criteria.A pattern of all don't cares means no channels are part of the pattern criteria, and therefore, there will be no triggers (unless Auto sweep triggers are enabled).
-
RSLope— Rising edge. -
FSLope— Falling edge. -
ESLope— Either edge.
The pattern can include an edge identifier on one channel only.