:TRIGger:SEQuence:TRANsition:MODE

Command Syntax

:TRIGger:SEQuence{A|B}:TRANsition:MODE  {TGTHan | TLTHan | RINSide | ROUTside}

Query Syntax

:TRIGger:SEQuence{A|B}:TRANsition:MODE?

Description

In the Edge Transition trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the edge transition time to trigger on:

Edges are identified when a signal passes through the trigger threshold voltage. The direction of the edge is determined based on hysteresis around the trigger threshold.